imx8 optee enanched OpenSSL example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8 optee enanched OpenSSL example

1,759 Views
matteo-facchinetti
Contributor II

Hi,

I'm interested to working with the Enhanced OpenSSL example (AN12632)
but with the iMX8 architecture.

When I try to compile optee-os with CFG_IMXCRYPT enabled, I give an error and then I see that this define is disabled by design when use it on iMX8

Is possible to use this example or any other similar (openssl+optee) with iMX8?

0 Kudos
Reply
1 Reply

1,724 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi matteo-facchinett,

 

For the moment there is no example as the optee is not supported on the imx8 devices.

 

Sorry for that.

Regards,

Israel.

0 Kudos
Reply