imx7d using dma to transfer eim data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx7d using dma to transfer eim data

2,415件の閲覧回数
864535720
Contributor II

Hello everyone
my development board is IMX7DSABRE. Linux kernel version is 4.9.88.
When I use dma to transmit EIM data to FPGA on imx7d, when I write data to EIM bus, some problems occur. My EIM bus data width is configured to 16bit, I write 16 bytes of data to the bus each time:
0x1234 0x1235 0x12346 0x1237 0x1238 0x1239 0x123a 0x123b
My FPGA can receive these 16 bytes of data, but it also receives an additional 16 bytes of 0 data. The 0 data was received because the EIM bus generated 8 more write signals.
Normally, according to the configuration of my data line width, when 16 bytes occur, only 8 write signals need to be generated, but actually 16 write signals are generated. The waveform diagram is as follows:

em4_snapshot_1594192757733.png


My dma code configuration is as follows:
dma_m2m_config.dst_addr_width = DMA_SLAVE_BUSWIDTH_2_BYTES;
dma_m2m_config.src_addr_width = DMA_SLAVE_BUSWIDTH_2_BYTES;
dma_m2m_config.src_maxburst = EIM_WRITE_SIZE/2;
dma_m2m_config.dst_maxburst = EIM_WRITE_SIZE/2;
dmaengine_slave_config(dma_m2m_chan, &dma_m2m_config);
dma_m2m_desc = dma_m2m_chan->device->device_prep_dma_memcpy(dma_m2m_chan, dma_dst, dma_src, length, DMA_MEM_TO_MEM);

I want to know why there are 16 write signals?

At the same time I tried to configure different values for dst_addr_width and src_addr_width, but no matter how I configure it, there will always be redundant write signals. How should I solve this problem?

At the same time I tried dst_addr_width and src_addr_width to configure different values, such as:
dma_m2m_config.dst_addr_width = DMA_SLAVE_BUSWIDTH_1_BYTE;
dma_m2m_config.src_addr_width = DMA_SLAVE_BUSWIDTH_1_BYTE;


dma_m2m_config.dst_addr_width = DMA_SLAVE_BUSWIDTH_1_BYTE;
dma_m2m_config.src_addr_width = DMA_SLAVE_BUSWIDTH_2_BYTES;


dma_m2m_config.dst_addr_width = DMA_SLAVE_BUSWIDTH_2_BYTES;
dma_m2m_config.src_addr_width = DMA_SLAVE_BUSWIDTH_1_BYTE;


dma_m2m_config.dst_addr_width = DMA_SLAVE_BUSWIDTH_2_BYTES;
dma_m2m_config.src_addr_width = DMA_SLAVE_BUSWIDTH_2_BYTES;


dma_m2m_config.dst_addr_width = DMA_SLAVE_BUSWIDTH_2_BYTES;
dma_m2m_config.src_addr_width = DMA_SLAVE_BUSWIDTH_4_BYTES;


dma_m2m_config.dst_addr_width = DMA_SLAVE_BUSWIDTH_4_BYTES;
dma_m2m_config.src_addr_width = DMA_SLAVE_BUSWIDTH_2_BYTES;


dma_m2m_config.dst_addr_width = DMA_SLAVE_BUSWIDTH_4_BYTES;
dma_m2m_config.src_addr_width = DMA_SLAVE_BUSWIDTH_4_BYTES;
But no matter how I configure it, there will always be redundant write signals. How should I solve this problem?

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,941件の閲覧回数
nx5216
Contributor I

HI,  did you solve the problem, now I have the same problem, could you tell me the solution. my email: [email protected]

0 件の賞賛
返信

2,375件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi  其东 刘

for eim burst with dma cases may be useful to look at

sect.9.7.5.4 Burst Clock Divisor (BCD), sect.9.7.5.8 AXI (Master) Bus Cycles Support

i.MX 7Dual Applications Processor Reference Manual

For example sdma source memory address was aligned according to burst size,

PSZ, BL settings in EIM_CSnGCR1 register. First may be useful to test configuration

with barmetal sdk:

rt-thread/eim_test.c at master · RT-Thread/rt-thread · GitHub 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
 

0 件の賞賛
返信