imx7d tce underrun problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx7d tce underrun problem

4,684件の閲覧回数
houyong
Contributor III

Dear nxp,

We use imx7d processor with eink 10.3 inch panel, and we are puzzled by the tce underrun problem.

We found that imx7d uboot has set the epdc qos priority like follows, but we do not know if it is right.

arch/arm/cpu/armv7/mx7/soc.c in u-boot:

static void set_epdc_qos(void)
{
#define REGS_QOS_BASE     QOSC_IPS_BASE_ADDR
#define REGS_QOS_EPDC     (QOSC_IPS_BASE_ADDR + 0x3400)
#define REGS_QOS_PXP0     (QOSC_IPS_BASE_ADDR + 0x2C00)
#define REGS_QOS_PXP1     (QOSC_IPS_BASE_ADDR + 0x3C00)

        writel(0, REGS_QOS_BASE);  /*  Disable clkgate & soft_reset */
        writel(0, REGS_QOS_BASE + 0x60);  /*  Enable all masters */
        writel(0, REGS_QOS_EPDC);   /*  Disable clkgate & soft_reset */
        writel(0, REGS_QOS_PXP0);   /*  Disable clkgate & soft_reset */
        writel(0, REGS_QOS_PXP1);   /*  Disable clkgate & soft_reset */

        writel(0x0f020722, REGS_QOS_EPDC + 0xd0);   /*  WR, init = 7 with red flag */
        writel(0x0f020722, REGS_QOS_EPDC + 0xe0);   /*  RD,  init = 7 with red flag */

        writel(1, REGS_QOS_PXP0);   /*  OT_CTRL_EN =1 */
        writel(1, REGS_QOS_PXP1);   /*  OT_CTRL_EN =1 */

        writel(0x0f020222, REGS_QOS_PXP0 + 0x50);   /*  WR,  init = 2 with red flag */
        writel(0x0f020222, REGS_QOS_PXP1 + 0x50);   /*  WR,  init = 2 with red flag */
        writel(0x0f020222, REGS_QOS_PXP0 + 0x60);   /*  rD,  init = 2 with red flag */
        writel(0x0f020222, REGS_QOS_PXP1 + 0x60);   /*  rD,  init = 2 with red flag */
        writel(0x0f020422, REGS_QOS_PXP0 + 0x70);   /*  tOTAL,  init = 4 with red flag */
        writel(0x0f020422, REGS_QOS_PXP1 + 0x70);   /*  TOTAL,  init = 4 with red flag */

        writel(0xe080, IOMUXC_GPR_BASE_ADDR + 0x0034); /* EPDC AW/AR CACHE ENABLE */
}

We also enable the priority elevation mechanism in linux kernel by set the EPDC register EPDC_FIFOCTRL bit31.

All above can not resolve the tce underrun problem, do you have some suggestions and experience?

Thanks a lot!

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

4,613件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Hou

nxp uboot has optimal epddc settings:

mx7dsabresd.c\mx7dsabresd\freescale\board - uboot-imx - i.MX U-Boot 

However for optimal performance of custom epd panel custom firmware may be needed,

as described in sect.6.4.5.8 Using a Custom Waveform File attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,613件の閲覧回数
houyong
Contributor III

Hi igorpadykov,

 

Thanks for your response!

But we have alreay used our custom firmware:epdc_ES103TC1.fw

And we got the tce underrun problem in linux kernel when app have updates, it is ok in uboot!

0 件の賞賛
返信

4,613件の閲覧回数
houyong
Contributor III

Hi igorpadykov,

Thanks for your response!

But we have alreay used our custom firmware:epdc_ES103TC1.fw

0 件の賞賛
返信