imx7d compatible MIPI camera and epdc.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx7d compatible MIPI camera and epdc.

2,942 Views
adnanali
Contributor III

Hello I want to know the compatible epdc and mipi-camera with imx7d sabre board. I have come to know that IMXEBOOKDC4 is compatible with imx7d sabre board, is it correct ? and also what is the compatible MIPI-camera with this target, will Nit6X_5MP_MIPI work ? Reference to product datasheet will be appreciated

hoping for a quick response.

thanks

Labels (3)
3 Replies

2,564 Views
gary_bisson
Senior Contributor III

Hi,

Regarding the camera, no the Nit6X_5MP_MIPI device isn't compatible with NXP SABRE design. However, it is compatible with all our products, including the Nitrogen7 (i.MX7) board:

https://boundarydevices.com/product/nitrogen7/

Regards,

Gary

2,564 Views
adnanali
Contributor III

Hello Gary, so can you please refer me to any MIPI camera that is compatible with the imx7d sabre design ?

0 Kudos
Reply

2,564 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Adnan Ali,

The i.MX7 SABRE SD has a MIPI CSI Port available for a Camera but there is not a designed Camera module for this port that I’m aware of. The board BSP does have dts files for the OV5640 but you would need to adapt the HW and then load the driver and appropriate dts in order to test the camera. I think some other customers have used the OV5647 MIPI camera successfully.

Regards,