phy detected as Generic PHY , link shows up , but no communication, link detection properly happening, on probing hardware ENET1_RGMII_TX_CTL / DATA no signals.
ENET1_RX_CTL / DATA signals ok
log shows:
30be0000.ethernet supply phy not found, using dummy regulator
[ 1.342383] fec 30be0000.ethernet eth0: registered PHC device 0
[ 1.350291] 30bf0000.ethernet supply phy not found, using dummy regulator
[ 1.362971] fec 30bf0000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
[ 1.373102] fec 30bf0000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: b2:18:cc:ce:62:bd
[ 1.403259] fec 30bf0000.ethernet eth1: registered PHC device 1
0.000000] Architected cp15 timer(s) running at 8.00MHz (phys).
[ 0.228980] 30800000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator
[ 0.229133] 30800000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator
[ 1.296217] libphy: Fixed MDIO Bus: probed
[ 1.316960] 30be0000.ethernet supply phy not found, using dummy regulator
[ 1.334155] libphy: fec_enet_mii_bus: probed
[ 1.350291] 30bf0000.ethernet supply phy not found, using dummy regulator
[ 1.397931] libphy: fec_enet_mii_bus: probed
fec 30bf0000.ethernet eth1: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=30be0000.etherne:01, irq=-1)
starting statd: [ 11.006923] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
fec 30bf0000.ethernet eth1: Link is Up - 1Gbps/Full - flow control rx/tx
[ 27.955314] IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready