imx6ull-yocto ddr3 porting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ull-yocto ddr3 porting

1,888 Views
li_hong
Contributor III

Hello Team,

     I have finished porting ddr3  from 512MiB to 1GiB successfully.I modified file "board/freescale/mx6ullevk/imximage.cfg" base on the parameters generated by  script "I.MX6ULL_DDR3_Script_Aid_V0.01.xlsx" and tool "ddr_stress_tester_v3.00". At the beginning,the board was unable to  start the kernel, and I try to comment uboot defconfig "CONFIG_IMX_OPTEE=y",it was able to start kernel normally.

    What I want to know is  what was the defconfig "CONFIG_IMX_OPTEE" used for and what  is the impact on the system when commenting the defconfig "CONFIG_IMX_OPTEE=y".

My develop environment:      

   Board:imx6ull

   Kernel:4.14.78

Thank you in advance.

Labels (2)
0 Kudos
Reply
1 Reply

1,818 Views
igorpadykov
NXP Employee
NXP Employee

Hi hong

for OPTEE usage one can look at sect.5.6.10 OP-TEE enablement

attached Yocto Guide, For memory check  #define PHYS_SDRAM_SIZE

mx6ullevk.h\configs\include - uboot-imx - i.MX U-Boot 

pay attention to cma size.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply