imx6ull start kernel fail from op-tee

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ull start kernel fail from op-tee

4,199 Views
kk163
Contributor III

Because the zImage size has increased, the FAT partition has been enlarged, so addr has been adjusted,

tee_addr=0x8b000000

fdt_addr=0x8a000000

Cause the kernel to fail to start ,if setenv tee =no kermel start succesfully

 

## Booting kernel from Legacy Image at 8b000000 ...
Image Name:
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1057044 Bytes = 1 MiB
Load Address: 84000000
Entry Point: 84000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 8a000000
Booting using the fdt blob at 0x8a000000
Loading Kernel Image
Using Device Tree in place at 8a000000, end 8a00bb93
Modify /soc/bus@2200000/epdc@228c000 disabled

why  Load Address & Entry Point   are  still the original default value 84000000, instead of 8b000000. How to modify it?

 

0 Kudos
Reply
5 Replies

4,171 Views
Yuri
NXP Employee
NXP Employee

@kk163 
Hello,

   Have You used recommendations of Chapter 5 (Configuring OP-TEE) in i.MX Porting Guide?

https://www.nxp.com/docs/en/user-guide/IMX_PORTING_GUIDE.pdf

 

Regards,
Yuri.

0 Kudos
Reply

4,137 Views
kk163
Contributor III

hi yuri
 According to IMX_PORTING_GUIDE.pdf, I finally found the location of the modification, modified the entry point address and solved the problem!! thank you!!

git\core\arch\arm\plat-imx\conf.mk
# put optee at DDR base address + 64MB for AARCH32
#CFG_TZDRAM_START ?= ($(CFG_DRAM_BASE) + 0x04000000)
CFG_TZDRAM_START ?= ($(CFG_DRAM_BASE) + 0x0B000000)


However, if the reboot  command is issued after modifying this entry point address , will the reboot  fail? Why is this?

root@imx6ull14x14evk:~# reboot
root@imx6ull14x14evk:~# [ OK ] Removed slice system-modprobe.slice.
[ OK ] Stopped target Multi-User System.
[ OK ] Stopped target Login Prompts.
[ OK ] Stopped target Network.
[ OK ] Stopped target Host and Network Name Lookups.
[ OK ] Stopped target Remote File Systems.
[ OK ] Stopped target RPC Port Mapper.
[ OK ] Stopped target Sound Card.
[ OK ] Stopped target System Time Synchronized.
[ OK ] Stopped target System Time Set.
[ OK ] Stopped target Timers.
[ OK ] Stopped Daily Cleanup of Temporary Directories.
[ OK ] Stopped target Hardware activated USB gadget.
Stopping Save/Restore Sound Card State...
Stopping Avahi mDNS/DNS-SD Stack...
Stopping Kernel Logging Service...
Mar 24 10:27:55 imx6ull14x14evk syslog.info syslogd exiting
Stopping System Logging Service...
Stopping D-Bus System Message Bus...
Stopping Getty on tty1...
Stopping Telephony service...
Stopping Serial Getty on ttymxc0...
Stopping Network Service...
Stopping Load/Save Random Seed...
Stopping TEE Supplicant...
[ OK ] Stopped Network Service.
[ OK ] Stopped Avahi mDNS/DNS-SD Stack.
[ OK ] Stopped Kernel Logging Service.
[ OK ] Stopped System Logging Service.
[ OK ] Stopped D-Bus System Message Bus.
[ OK ] Stopped Getty on tty1.
[ OK ] Stopped Telephony service.
[ OK ] Stopped Serial Getty on ttymxc0.
[ OK ] Stopped TEE Supplicant.
[ OK ] Stopped Save/Restore Sound Card State.
[ OK ] Stopped Load/Save Random Seed.
[ OK ] Removed slice system-getty.slice.
[ OK ] Removed slice system-serial\x2dgetty.slice.
[ OK ] Stopped target Basic System.
[ OK ] Stopped target Paths.
[ OK ] Stopped Dispatch Password …ts to Console Directory Watch.
[ OK ] Stopped Forward Password R…uests to Wall Directory Watch.
[ OK ] Stopped target Slices.
[ OK ] Removed slice User and Session Slice.
[ OK ] Stopped target Sockets.
[ OK ] Closed Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Closed D-Bus System Message Bus Socket.
[ OK ] Stopped target System Initialization.
[ OK ] Closed Syslog Socket.
Stopping Load/Save Screen …backlight:backlight-display...
[ OK ] Stopped Apply Kernel Variables.
[ OK ] Stopped Update is Completed.
[ OK ] Stopped Rebuild Dynamic Linker Cache.
[ OK ] Stopped Rebuild Journal Catalog.
[ OK ] Stopped Create Volatile Files and Directories.
[ OK ] Stopped target Local File Systems.
Unmounting Temporary Directory (/tmp)...
Unmounting /var/volatile...
[ OK ] Stopped Load/Save Screen B…f backlight:backlight-display.
[ OK ] Unmounted Temporary Directory (/tmp).
[ OK ] Unmounted /var/volatile.
[ OK ] Removed slice system-systemd\x2dbacklight.slice.
[ OK ] Stopped target Local File Systems (Pre).
[ OK ] Stopped target Swap.
[ OK ] Reached target Unmount All Filesystems.
[ OK ] Stopped Create Static Device Nodes in /dev.
[ OK ] Stopped Create System Users.
[ OK ] Stopped Remount Root and Kernel File Systems.
[ OK ] Reached target Shutdown.
[ OK ] Reached target Final Step.
[ OK ] Finished Reboot.
[ OK ] Reached target Reboot.
[ 170.998048] watchdog: watchdog0: watchdog did not stop!
[ 171.033471] systemd-shutdown[1]: Syncing filesystems and block devices.
[ 171.042851] systemd-shutdown[1]: Sending SIGTERM to remaining processes...
[ 171.067166] systemd-journald[117]: Received SIGTERM from PID 1 (systemd-shutdow).
[ 171.093893] systemd-shutdown[1]: Sending SIGKILL to remaining processes...
[ 171.115632] systemd-shutdown[1]: Using hardware watchdog 'imx2+ watchdog', version 0, device /dev/watchdog
[ 171.131600] systemd-shutdown[1]: Unmounting file systems.
[ 171.141514] [198]: Remounting '/' read-only in with options '(null)'.
[ 171.149145] systemd-shutdown[1]: All filesystems unmounted.
[ 171.155328] systemd-shutdown[1]: Deactivating swaps.
[ 171.160880] systemd-shutdown[1]: All swaps deactivated.
[ 171.166155] systemd-shutdown[1]: Detaching loop devices.
[ 171.181098] systemd-shutdown[1]: All loop devices detached.
[ 171.186728] systemd-shutdown[1]: Stopping MD devices.
[ 171.192847] systemd-shutdown[1]: All MD devices stopped.
[ 171.198212] systemd-shutdown[1]: Detaching DM devices.
[ 171.204392] systemd-shutdown[1]: All DM devices detached.
[ 171.209848] systemd-shutdown[1]: All filesystems, swaps, loop devices, MD devices and DM devices detached.
[ 171.224121] systemd-shutdown[1]: Syncing filesystems and block devices.
[ 171.233279] systemd-shutdown[1]: Rebooting.
[ 171.263646] ci_hdrc ci_hdrc.1: remove, state 4
[ 171.268130] usb usb1: USB disconnect, device number 1
[ 171.274449] ci_hdrc ci_hdrc.1: USB bus 1 deregistered
[ 171.297357] imx2-wdt 20bc000.watchdog: Device shutdown: Expect reboot!
[ 171.304882] reboot: Restarting system
[ 172.309040] Reboot failed -- System halted

 

CFG_TZDRAM_START ?= ($(CFG_DRAM_BASE) + 0x04000000)
reboot is ok!!

CFG_TZDRAM_START ?= ($(CFG_DRAM_BASE) + 0x0B000000)

reboot failed!!

 

 

4,134 Views
Yuri
NXP Employee
NXP Employee

@kk163 
Hello,

  usually it is recommended to provide total system Power On Reset if system should be
reboot - in order to avoid iMX  boot issues, when power is not removed from all board 
components.

  Is it implemented on Your board?

Regards,
Yuri.

0 Kudos
Reply

4,128 Views
kk163
Contributor III

Yes, it was implemented on the imx6ullevk board. The customer raised this question and wanted to know what caused the reboot fail after CFG_TZDRAM_START ?= ($(CFG_DRAM_BASE) + 0x0B000000) ?

thanks!

0 Kudos
Reply

4,185 Views
kk163
Contributor III

@Yuri ,please help! thank you!

0 Kudos
Reply