imx6ull sd2 pins for default boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6ull sd2 pins for default boot

3,368 次查看
harshakumar
Contributor II

In MCIMX6ULL-CM EVM schematic NAND Flash and SD2 lines are muxed. But for my custom design require dedicated NAND Flash and eMMC. Hence SD2 lines for eMMC taken from LCD lines.

Is still eMMC boot configuration works ?,  as I moved the eMMC lines from NAND to LCD lines any other changes to do for booting from emmc ?

Thanks

Harsha

标签 (2)
1 回复

3,260 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Harsha

for available eMMC boot configurations one can look on

sect.8.5.3.4 IOMUX configuration for SD/MMC i.MX6ULL Reference Manual 

http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------