imx6ull Custom Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ull Custom Board

1,420 Views
ylmzhsn_
Contributor III

Hi NXP,

I have the okimx6ull-s system on module. 

https://www.forlinx.net/product/i.mx6ull-system-on-module-106.html

I'm trying to program emmc but I'm getting an error:

                                                                              
U-Boot 2022.04-lf_v2022.04+g16e8414193 (Oct 08 2022 - 13:33:43 +0000)           
                                                                                
CPU:   i.MX6ULL rev1.1 792 MHz (running at 396 MHz)                             
CPU:   Industrial temperature grade (-40C to 105C) at 42C                       
Reset cause: POR                                                                
Model: i.MX6 ULL 14x14 EVK Board                                                
Board: MX6ULL 14x14 EVK                                                         
DRAM:  512 MiB                                                                  
Core:  65 devices, 18 uclasses, devicetree: separate                            
MMC:   FSL_SDHC: 0, FSL_SDHC: 1                                                 
Loading Environment from MMC... *** Warning - bad CRC, using default environment
                                                                                
[*]-Video Link 0 (480 x 272)                                                    
        [0] lcdif@21c8000, video                                                
In:    serial                                                                   
Out:   serial                                                                   
Err:   serial                                                                   
switch to partitions #0, OK                                                     
mmc1(part 0) is current device                                                  
flash target is MMC:1                                                           
Net:   Could not get PHY for FEC1: addr 1                                       
Could not get PHY for FEC1: addr 1                                              
Get shared mii bus on ethernet@2188000       

Works in original software :

MMC:   FSL_SDHC: 0, FSL_SDHC: 1                               
Display: TFT70AB-1024x600                                                       
Video: 1024x600x24                                                              
Card did not respond to voltage select!                                         
reading logo.bmp                                                                
391736 bytes read in 24 ms (15.6 MiB/s)                                         
In:    serial                                                                   
Out:   serial                                                                   
Err:   serial                                                                   
Time-out: 128s                                                                  
switch to partitions #0, OK                                                     
mmc1(part 0) is current device                                                  
Saving Environment to MMC...                                                    
Writing to MMC(1)... done                                                       
Saving Environment to MMC...                                                    
Writing to MMC(1)... done                                                       
                                                                                
Warning: MAC address is generated using cpuid                                   
Net:   Board Net Initialization Failed                                          
No ethernet found.                                                              
Normal Boot                                                                     
Press SPACE to abort autoboot in 1 seconds                                      
reading boot.scr                      

my yocto project file:

        $ mkdir imx-yocto-bsp
	$ cd imx-yocto-bsp
	$ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.52-2.1.0.xml
	$ repo sync
	$ DISTRO=fsl-imx-wayland MACHINE=imx6ull14x14evk source imx-setup-release.sh -b build
	$ bitbake imx-image-core

How do I create my own yocto project for my custom card? 

 

0 Kudos
Reply
1 Reply

1,404 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You have to adapt the driver and its programming to your pcb, check your device tree the locations of all modules.

Regards

0 Kudos
Reply