imx6ul with quad spi support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6ul with quad spi support

跳至解决方案
3,038 次查看
keithmo
Contributor II

Hello,

I'm currently trying to read a quad spi flash (mt25ql128) in linux (kernel 4.1.15) with imx6ul chip. However, it seems only the pin used for 1-bit width is flipping properly.

Below are relevant parts from my device tree:

                pinctrl_qspi: qspigrp {
                        fsl,pins = <
                                MX6UL_PAD_NAND_WP_B__QSPI_A_SCLK        0x00007088
                                MX6UL_PAD_NAND_READY_B__QSPI_A_DATA00   0x00007088
                                MX6UL_PAD_NAND_CE0_B__QSPI_A_DATA01     0x00007088
                                MX6UL_PAD_NAND_CE1_B__QSPI_A_DATA02     0x00007088
                                MX6UL_PAD_NAND_CLE__QSPI_A_DATA03       0x00007088
                                MX6UL_PAD_NAND_DQS__QSPI_A_SS0_B        0x00007088
                        >;
                };
&qspi {
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_qspi>;
        status = "okay";
        flash0: mt25ql128ab@0 {
                #address-cells = <1>;
                #size-cells = <1>;
                compatible = "micron,n25q128a13", "jedec,spi-nor";
                /*spi-tx-bus-width = <4>;*/
                spi-rx-bus-width = <4>;
                spi-max-frequency = <10000000>;
                reg = <0>;
                partition@0x00000000 {
                        label = "parta";
                        reg = <0x00000000 0xC0000>;
                };
                partition@0x000C0000 {
                        label = "partb";
                        reg = <0x000C0000 0x0>;
                };
        };
};

Dmesg appears to show the flash being detected successfully, but when I read from the device, only bit 1 is switching properly. All other bits (0, 2, 3) appear to be constant low. This results in values such as 0xFF being read as 0x22, or 0x12 as 0x02 (I believe.)

fsl-quadspi 21e0000.qspi: n25q128a13 (16384 Kbytes)
2 ofpart partitions found on MTD device 21e0000.qspi
Creating 2 MTD partitions on "21e0000.qspi":
0x000000000000-0x0000000c0000 : "parta"
0x0000000c0000-0x000001000000 : "partb"

Any help would be appreciated, thanks!
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,005 次查看
keithmo
Contributor II

Hello,

Just an update, I found this posting from Marcus saying the controller is left in DDR mode if booting from qspi, which is also my case.

https://community.nxp.com/thread/429073

I had to reconfigure everything for DDR and now it works.

Thanks for your time.

在原帖中查看解决方案

2 回复数
2,005 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keith

one can try with  nxp bsp releases and use imx6ul-14x14-evk.dts:
http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6ul-14x14-evk.dts?...
documentation in fsl-quadspi.txt:
http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/Documentation/devicetree/bindings/mtd/f...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,006 次查看
keithmo
Contributor II

Hello,

Just an update, I found this posting from Marcus saying the controller is left in DDR mode if booting from qspi, which is also my case.

https://community.nxp.com/thread/429073

I had to reconfigure everything for DDR and now it works.

Thanks for your time.