imx6ul spi communication with buffer IC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul spi communication with buffer IC

1,524 Views
surendradhobale
Contributor III

Hello,

      We are using the imx6ul based custom board. We are require multiple Serial Port (RS485), so used MAX14830 expansion chip to achive the ports on the SPI.

To get good signal strength we have added one buffer IC in betwen the CPU board and SPI-UART expander ( MAX14830).

But currently problem is, the communicaion is working very fine without the buffer.( as shown in below 2nd diagram)

but not reliable communication with 1st diagram setup.

We are looking to use the buffer in our setup.

What kind of the timing related changes required for same on SPI or Max14830 driver?

We are using 4.1.15 or 4.9 kernel (both having same behaviour).

Kindly help , if we are looking to add the buffer IC, what kind of changes required either in software side (i.e in linux kernel).

Setup.png

Regards,

Surendra

Labels (3)
0 Kudos
Reply
1 Reply

1,307 Views
igorpadykov
NXP Employee
NXP Employee

Hi Surendra

one can check with oscilloscope ecspi timings and compare with good setup,

in particular CS8 -  ECSPIx_MISO Setup Time, described in

Table 47. ECSPI Master Mode Timing Parameters i.MX6UL Datasheet
http://www.nxp.com/docs/en/data-sheet/IMX6ULCEC.pdf

these timings are hardware timings and can not be changed by software.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------