imx6ul: Uboot initializes LCDIF exceptions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6ul: Uboot initializes LCDIF exceptions

1,969件の閲覧回数
244143298
Contributor I

Board:imx6ul  When UBOOT resets LCDIF block, what is the reason for clkgate setting failure

  • When the LCDIF register is normal, the status is c0000000

  • When the LCDIF register is abnormal, the state is 80000000

 

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,820件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 我的钱 去玩儿群无

LCD clocks are enabled in CCM_CCGR2 register described in

sect.18.6.25 CCM Clock Gating Register 2 (CCM_CCGR2)

i.MX 6UltraLite Applications Processor Reference Manual

clocks can be enabled in dcd header:

imximage.cfg\mx6ullevk\freescale\board - uboot-imx - i.MX U-Boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,820件の閲覧回数
244143298
Contributor I

Current situation: Why does the CLkgate bit not set 1 when UBOOT resets the LCDIF block device

0 件の賞賛
返信