imx6qsabresd Linux remote file access and Eclipse debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6qsabresd Linux remote file access and Eclipse debug

1,973件の閲覧回数
ritesh_panchal
Contributor I

I am using imx6qsabresd board running fsl-image-multimedia-full linux 3.14.28 based image.

I want to access my board file system remotely over ethernet/usb.

So tell me the procedure how to access? or which packages i need to add in image?

And another i am using eclipse for cross compiling application for the board. I want to debug my application on my board from eclipse on my PC.

I configured ssh and gdb as per the yocto manual. But i think there are some package missing in my linux image.

So what's the procedure to enable this?

ラベル(4)
0 件の賞賛
返信
3 返答(返信)

1,759件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Add this to your conf/local.conf

EXTRA_IMAGE_FEATURES = "debug-tweaks tools-debug eclipse-debug ssh-server-openssh"

CORE_IMAGE_EXTRA_INSTALL += "openssh-sftp openssh-sftp-server"

Regards,

Luis

0 件の賞賛
返信

1,759件の閲覧回数
b36401
NXP Employee
NXP Employee

You can configure ftp server on the board and access the filesystem from the outside of the board via ftp.

And you can use gdbserver for remote debugging the applications.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,759件の閲覧回数
ritesh_panchal
Contributor I

i have configure ssh server. and able to access file system using sftp://root@ip_address:28.

But how to create ftp server?

i followed the below link to debug hello world application from eclipse.

http://developer.toradex.com/knowledge-base/hello-world-application-on-embedded-linux​

Eclipse generate .o file. But how to generate .ko using eclipse?

0 件の賞賛
返信