imx6q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q

3,346件の閲覧回数
一个人的城市
Contributor I

Hello!I created image,and the kernel version is 4.1.15.I use this command:DISTRO=fsl-imx-x11 MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-x11 and bitbake fsl-image-qt5;but after starting,i want to show my own desktop,For example, a simple QT program,what should i do?I am a novice ,I hope you can give me some advices.Thanks

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,461件の閲覧回数
b36401
NXP Employee
NXP Employee

You need to add your application to startup for it ru run automatically when the OS starts up.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,461件の閲覧回数
一个人的城市
Contributor I

Where to add? And where is the desktop system started?Can you tell me in detail!Thanks

0 件の賞賛
返信