imx6q weston error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q weston error

2,599 次查看
anabitatropos
Contributor I

hello all:

BSP 4.1.15_1.1.0

root@imx6qsabresd:~# weston --tty=1 &                                                                                                      

[1] 793                                                                                                                                    

root@imx6qsabresd:~# Date: 2016-05-16 UTC                                                                                                  

[06:17:52.106] weston 1.9.0                                                                                                                

               http://wayland.freedesktop.org                                                                                              

               Bug reports to: https://bugs.freedesktop.org/enter_bug.cgi?product=Wayland&component=weston&version=1.9.0                   

               Build: 1.8.93-2-gb05cdb8 configure.ac: bump to version 1.9.0 for the official release (2015-09-21 18:11:26 -0700)           

[06:17:52.107] OS: Linux, 3.10.45, #212 SMP PREEMPT Mon Jan 4 15:07:39 CST 2016, armv7l                                                    

[06:17:52.107] warning: XDG_RUNTIME_DIR "/var/run/user/1000" is not configured                                                             

correctly.  Unix access mode must be 0700 (current mode is 755),                                                                           

and must be owned by the user (current owner is UID 0).                                                                                    

Refer to your distribution on how to get it, or                                                                                            

http://www.freedesktop.org/wiki/Specifications/basedir-spec                                                                                

on how to implement it.                                                                                                                    

[06:17:52.109] Starting with no config file.                                                                                               

[06:17:52.109] Loading module '/usr/lib/weston/fbdev-backend.so'                                                                           

[06:17:52.133] Output repaint window is 7 ms maximum.                                                                                      

[06:17:52.133] initializing fbdev backend                                                                                                  

[06:17:52.135] Loading module '/usr/lib/weston/gl-renderer.so'                                                                             

[06:17:52.137] warning: either no EGL_EXT_platform_base support or specific platform support; falling back to eglGetDisplay.               

*** Error in `weston': free(): invalid pointer: 0x014af61c ***                                                                             

                                                                                                                                           

[1]+  Aborted                 weston --tty=1 

标签 (2)
0 项奖励
回复
1 回复

1,608 次查看
b36401
NXP Employee
NXP Employee

Please refer this document regarding to building Wayland-Weston server:

https://community.freescale.com/docs/DOC-95380

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复