imx6q porting issure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q porting issure

1,294 Views
xulj
Contributor I

hi,

I have an issure when i was buildig image of linux kernel 3.10.17 by using yocto project, the reference doc is 《Freescale Yocto Project User's Guide》

 

when i run the command

$bitbake fsl-image-x11

it returns error as autotools.patch failed,more details pls see the attachment.thanks

Original Attachment has been moved to: log.do_patch.2756.zip

Labels (2)
0 Kudos
Reply
1 Reply

1,178 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Before you build your images, have you installed sucssesful the host packages for your Ubuntu host setup, in the 3.1 Host packages, you can see the detail command.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply