imx6q porting issure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q porting issure

1,302件の閲覧回数
xulj
Contributor I

hi,

I have an issure when i was buildig image of linux kernel 3.10.17 by using yocto project, the reference doc is 《Freescale Yocto Project User's Guide》

 

when i run the command

$bitbake fsl-image-x11

it returns error as autotools.patch failed,more details pls see the attachment.thanks

Original Attachment has been moved to: log.do_patch.2756.zip

ラベル(2)
0 件の賞賛
返信
1 返信

1,186件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Before you build your images, have you installed sucssesful the host packages for your Ubuntu host setup, in the 3.1 Host packages, you can see the detail command.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信