imx6q lvds和hdmi双屏同显

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q lvds和hdmi双屏同显

8,452 Views
jakiewen
Contributor I

公司产品医疗电子行业,linux4.1.15+qt系统,需要屏幕lvds主显和hdmi线接出屏同时显示一个应用程序的输出

目前我们的uboot设置如下

root@Summer:~# fw_printenv mmcroot

mmcroot=/dev/mmcblk3p2 rootwait rw

root@Summer:~# fw_printenv mxcfb0

mxcfb0=video=mxcfb0:dev=ldb,1920x1080@60,if=RGB888,bpp=16

root@Summer:~# fw_printenv mxcfb1

mxcfb1=video=mxcfb1:dev=hdmi,1920x1080@60,if=RGB24,bpp=24

root@Summer:~# fw_printenv mxcfb2 

mxcfb2=video=mxcfb2:off

root@Summer:~# fw_printenv mxcfb3

mxcfb3=video=mxcfb3:off

经查,这样设置没有效果,主要主屏输出lvds,hdmi不输出;

设置fb0为hdmi,fb1为lvds,则主要输出在hdmi,lvds没有输出;

设置fb0为lvds,fb2为hdmi,则默认只输出lvds(因为qt程序默认用的fb0输出)

开启两个进程分别输出到fb0和fb2,则两个屏幕都能输出但是不是同一个内容;

请教下是否有解决方案

Labels (1)
0 Kudos
Reply
7 Replies

6,502 Views
yyuan
Contributor III

你好  

我现在也遇到了这个问题  我的是lcd+hdmi,你的问题解决了吗?

我的hdmi是fb1,

谢谢啦  

0 Kudos
Reply

6,502 Views
jakiewen
Contributor I

linux+ qt

uboot para:

1.

fw_setenv mmcroot '/dev/mmcblk3p2 video=mxcfb0:dev=ldb,1280x800M@60,if=RGB666,bpp=32 video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb2:off video=mxcfb3:off ldb=dul1 rootwait rw'
We could get lvds output, but hdmi does't output.

2.

fw_setenv mmcroot '/dev/mmcblk3p2 video=mxcfb1:dev=ldb,1280x800M@60,if=RGB666,bpp=32 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb2:off video=mxcfb3:off ldb=dul1 rootwait rw' 

We could get hdmi output, lvds does't output.

3.

fw_setenv mmcroot '/dev/mmcblk3p2 video=mxcfb0:dev=ldb,1280x800M@60,if=RGB666,bpp=32 video=mxcfb2:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb1:off video=mxcfb3:off ldb=dul1 rootwait rw' 

We could get hdmi output and lvds output by two different qt process seperately.

So how can i get both lvds and hdmi output at the same time by one process?

0 Kudos
Reply

6,502 Views
joanxie
NXP TechSupport
NXP TechSupport

did you check your ipu_id and disp_id in your source code? try not to set them in the same ipu, and could you give me the log file of command 1 and command 2?

0 Kudos
Reply

6,502 Views
jakiewen
Contributor I

1.how to check this,driver code or dtsi?

2.which log do you want?kernel  startup log?

0 Kudos
Reply

6,502 Views
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the topic :

https://community.nxp.com/thread/311751 

0 Kudos
Reply

6,502 Views
yitang
Contributor I

it is same setting for Android  like ubuntu,is right?

0 Kudos
Reply

6,501 Views
yitang
Contributor I

hi 俊凯 文:

   i had the same problem, how did you solved it in the end?

0 Kudos
Reply