imx6q-kernel not starting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q-kernel not starting

5,798件の閲覧回数
bhupeshpatil
Contributor I

I am working on the custom board using iMX6q. Following is hardware detail

a. Processor name : MCIMX6Q6AVT10AC

b. Nor Flash : S29GL01GS

c. DDR3 memory : MT41K128M16

d. emmc card : N2M400JD

e. ARM Audio Codec : SGTL500

f. UART : MAX3232

g. LVDS Display : PD050VL1


I am using NOR flash as a booting device. I  am using SABRE AI bsp. The uboot is modified according to hardware and is functional. Kernel image is also downloaded into the flash. The kernel gets loaded but execution is not happening .


Following is the console

U-Boot 2009.08 (Feb 27 2014 - 21:39:10)

CPU: Freescale i.MX6 family TO1.2 at 792 MHz

Thermal sensor with ratio = 179

Temperature:   42 C, calibration data 0x56b4b27d

mx6q pll1: 792MHz

mx6q pll2: 528MHz

mx6q pll3: 480MHz

mx6q pll8: 50MHz

ipg clock     : 66000000Hz

ipg per clock : 66000000Hz

uart clock    : 80000000Hz

cspi clock    : 60000000Hz

ahb clock     : 132000000Hz

axi clock   : 264000000Hz

emi_slow clock: 132000000Hz

ddr clock     : 528000000Hz

usdhc1 clock  : 198000000Hz

usdhc2 clock  : 198000000Hz

usdhc3 clock  : 198000000Hz

usdhc4 clock  : 198000000Hz

nfc clock     : 24000000Hz

Board: i.MX6Q-SABREAUTO: unknown-board Board: 0x63012 [POR]

Boot Device: NOR

I2C:   Hello i am  in I2c DRIVER

ready

MX6Q Configuring I2C2...

i2c pinmux set

I2C2 Clock enabled

Calling Audio Code...Hello i am  in I2c DRIVER

i2c_read chip: 0x0a addr: 0x0000 alen: 2 len: 2

CR=a0

Audio dev id: 0xa0

Audio dev id: 0x11

DRAM:   2 GB

Calling Display Flash Config Fn

Executing Flash init

Calling Get Size

BANK_BASE = 0x08000000

Executing Get_size

flash detect cfi

fwc addr 08000000 cmd f0 f0 8bit x 8 bit

fwc addr 08000000 cmd ff ff 8bit x 8 bit

fwc addr 08000055 cmd 98 98 8bit x 8 bit

is= cmd 51(Q) addr 08000010 is= 0 51

fwc addr 08000555 cmd 98 98 8bit x 8 bit

is= cmd 51(Q) addr 08000010 is= 0 51

Error in ___Flash_Detect_cfi

fwc addr 08000000 cmd f0 f0f0 16bit x 8 bit

fwc addr 08000000 cmd ff ffff 16bit x 8 bit

fwc addr 080000aa cmd 98 9898 16bit x 8 bit

is= cmd 51(Q) addr 08000020 is= 0051 5151

fwc addr 08000aaa cmd 98 9898 16bit x 8 bit

is= cmd 51(Q) addr 08000020 is= 0051 5151

Error in ___Flash_Detect_cfi

fwc addr 08000000 cmd f0 00f0 16bit x 16 bit

fwc addr 08000000 cmd ff 00ff 16bit x 16 bit

fwc addr 080000aa cmd 98 0098 16bit x 16 bit

is= cmd 51(Q) addr 08000020 is= 0051 0051

is= cmd 52(R) addr 08000022 is= 0052 0052

is= cmd 59(Y) addr 08000024 is= 0059 0059

device interface is 1

found port 2 chip 2 port 16 bits chip 16 bits

CFI_CMDSET_AMD_STANDARD

CFI_CMDSET_AMD_EXTENDED

fwc addr 08000000 cmd f0 00f0 16bit x 16 bit

fwc addr 08000aaa cmd aa 00aa 16bit x 16 bit

fwc addr 08000554 cmd 55 0055 16bit x 16 bit

fwc addr 08000aaa cmd 90 0090 16bit x 16 bit

fwc addr 08000000 cmd f0 00f0 16bit x 16 bit

fwc addr 080000aa cmd 98 0098 16bit x 16 bit

flash_fixup_amd

manufacturer is 2

manufacturer id is 0x1

device id is 0x227e

device id2 is 0x0

cfi version is 0x3135

fwc addr 08000000 cmd f0 00f0 16bit x 16 bit

Flash: 128 MB

MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3

Hello i am  in I2c DRIVER

In:    serial

Out:   serial

Err:   serial

Net:   got MAC address from IIM: 00:00:00:00:00:00

FEC0 [PRIME]

Hit any key to stop autoboot:  0

## Booting kernel from Legacy Image at 10800000 ...

   Image Name:   Linux-3.0.35-2666-gbdde708

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    3866700 Bytes =  3.7 MB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... OK

   Loading Kernel Image ... OK

OK

Starting kernel ...

What could be reason that kernel gets hang?
0 件の賞賛
返信
9 返答(返信)

4,923件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

could it be the console setting wrong? ttymxc3 for AI board?

4,923件の閲覧回数
bhupeshpatil
Contributor I

Thanks!!

I have shifted back to ttymxc3. Now I am one step forward. Following is the console,

Starting kernel ...

Uncompressing Linux... done, booting the kernel.

But the problem is only tx pin is available and I can't use this port. I am using  ttymxc0. If I modify the uboot for ttmxc0, it works upto uboot. But when I modify the kernel for ttymxc0, kernel staring message come and hangs. Even if i shifted back kernel to ttymxc3, same is the result.

Can you please tell the correct settings for uboot and kernel for changing serial console to ttymxc0?

0 件の賞賛
返信

4,923件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

maybe you can try enable early printk to see where did it hang, to enable early printk, please search it in kernel menuconfig, it should be inside kernel hack item....check it, and then add "earlyprintk" in your uboot commandline, then there should be more log output.

0 件の賞賛
返信

4,923件の閲覧回数
bhupeshpatil
Contributor I

We are now successful in using ttymxc0. We have done settings to enable early printk. how to add earlyprintk in uboot commandline?

0 件の賞賛
返信

4,923件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

in uboot, use "pri", then find the bootargs_base, add "earlyprintk" into it.

0 件の賞賛
返信

4,923件の閲覧回数
bhupeshpatil
Contributor I

we have modified imx6q_sabreauto_weimnor.h to add earlyprintk. we have used pri, following is the setting.

Hit any key to stop autoboot:  0

MX6Q SABREAUTO U-Boot > pri

bootdelay=3

baudrate=115200

ipaddr=192.168.1.103

serverip=192.168.1.101

netmask=255.255.255.0

loadaddr=0x10800000

netdev=eth0

ethprime=FEC0

uboot=u-boot.bin

kernel=uImage

nfsroot=/opt/eldk/arm

bootargs_base=setenv bootargs earlyprintk console=ttymxc0,115200

bootcmd=run bootcmd_nor

bootargs_nor=setenv bootargs ${bootargs} root=/dev/nfs  ip=dhcp weim-nor nfsroot=${serverip}:${nfsroot},v3,tcp

bootcmd_nor=run bootargs_base bootargs_nor;     cp.l 0x8080000 ${loadaddr} 0x400000; bootm

stdin=serial

stdout=serial

stderr=serial

ethac

0 件の賞賛
返信

4,923件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Have you enable the early printk in your linux menu config during compiling the uImage?

0 件の賞賛
返信

4,923件の閲覧回数
bhupeshpatil
Contributor I

yes, printk is enabled in the linux menu config.

in our hardware there is no LAN connected as well as no ramdisk image saved

0 件の賞賛
返信

4,923件の閲覧回数
bhupeshpatil
Contributor I

does dtb also required ?

0 件の賞賛
返信