imx6q ibis model

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q ibis model

1,699 次查看
vikashchandra
Contributor I

hi,

Could any body provide me ibis model of IMX6Q , Website's Ibis model is not correct, if any model there can use instead of.

Please share the link and any information. or can send my email id vikash_chandra1988will be thankful of you.

BR

0 项奖励
回复
6 回复数

1,464 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vikash

why do you think that it is not correct, it is validated before

release. For usage one can look at sect.9.7 IBIS usage

i.MX6 System Development User’s Guide (rev.1, 6/2013)

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

in particular:

Freescale board designers used the i.MX6Q IBIS model with the Hyperlynx tool

by Mentor Graphics. The HyperLynx version used was HyperLynx v8.1.1 + Update 2.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,464 次查看
vikashchandra
Contributor I

Dear Igor,

Thanks a ton for your valuable reply, The ibis model is fine but the

problem is in when we use it show the IC B3 pin is NC but in our design

this pin is not NC,it connected with NET,

For your reference attaching the snapshot.

BR

Vikash Chandra

0 项奖励
回复

1,464 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vikash

right, IC B3 pin is PCIE_TXP not supported by ibis model,

this is described in Table 9-6. i.MX6 pins not supported by IBIS

i.MX6 System Development User’s Guide

~igor

0 项奖励
回复

1,464 次查看
vikashchandra
Contributor I

Hi Igor,

Is the Ibis editor can help because during assignment of ibis model it

shows error.Trying but I don't think so it will help me.

So please provide me any solution on it if you have.

It will help me , would be ton of thanks for you.

BR

Vikash

0 项奖励
回复

1,464 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vikash

this may depend on ibis software, I think you should

read its documentation how to handle with unused pins.

As a workaround one can remove (comment) the [Diff Pin]

entries in the IBIS file for  the problematic pins.

Example :

[Diff Pin]  inv_pin  vdiff  tdelay_typ tdelay_min tdelay_max

A6          B6       NA        NA        NA        NA  

Best regards

igor

0 项奖励
回复

1,464 次查看
vikashchandra
Contributor I

Dear Igor,

Appreciate your prompt reply.

So What I should to do know, Can use any other instead of IMX6Q, If have

any Idea please provide..

Once thank you very much for help.

BR

Vikash

0 项奖励
回复