hi,
Could any body provide me ibis model of IMX6Q , Website's Ibis model is not correct, if any model there can use instead of.
Please share the link and any information. or can send my email id vikash_chandra1988will be thankful of you.
BR
Hi Vikash
why do you think that it is not correct, it is validated before
release. For usage one can look at sect.9.7 IBIS usage
i.MX6 System Development User’s Guide (rev.1, 6/2013)
http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf
in particular:
Freescale board designers used the i.MX6Q IBIS model with the Hyperlynx tool
by Mentor Graphics. The HyperLynx version used was HyperLynx v8.1.1 + Update 2.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Vikash
right, IC B3 pin is PCIE_TXP not supported by ibis model,
this is described in Table 9-6. i.MX6 pins not supported by IBIS
i.MX6 System Development User’s Guide
~igor
Hi Igor,
Is the Ibis editor can help because during assignment of ibis model it
shows error.Trying but I don't think so it will help me.
So please provide me any solution on it if you have.
It will help me , would be ton of thanks for you.
BR
Vikash
Hi Vikash
this may depend on ibis software, I think you should
read its documentation how to handle with unused pins.
As a workaround one can remove (comment) the [Diff Pin]
entries in the IBIS file for the problematic pins.
Example :
[Diff Pin] inv_pin vdiff tdelay_typ tdelay_min tdelay_max
A6 B6 NA NA NA NA
Best regards
igor
Dear Igor,
Appreciate your prompt reply.
So What I should to do know, Can use any other instead of IMX6Q, If have
any Idea please provide..
Once thank you very much for help.
BR
Vikash