Hi,
I am having graphics related issues (GPU hangs while running vivante samples) with L3.10.17_1.0.0_ga (vivante driver ver 4.6.9.9754) and I believe it is coming from the GPU driver. So, as an experiment I would like to try Linux imx_3.10.31_1.1.0_beta2 that uses later vivante drivers (5.0.11.p1.19959) . Hopefully the new driver solves the bug.
Can someone point out the steps to build the BSP (vivante framebuffer build) for imx6qsabresd that uses the latest gpu drivers?
(I'm using a third party board which is based on imx6qsabresd).
Any inputs will be of help!.
-Pj