imx6q eim problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q eim problem

271 Views
xjy198903
Contributor III

 

The EIM module of imx6q uses a 16-bit address line (AD0~AD15),16-bit data line (DA16~DA31), asynchronous mode, the module is connected to FPGA, no matter it is read or write, the information on the data line is valid, but there is always no valid data on the address line, the module is connected to FPGA, no matter it is read or write, the information on the data line is valid, but there is always no valid data on the address line.

 
Tags (1)
0 Kudos
Reply
0 Replies