imx6q boot from emmc failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q boot from emmc failed

1,759件の閲覧回数
yacheng_zhang
Contributor I

Hello, technical support:

      I made a imx6q board,When emmc works at 52m clock, it can't start properly. Manually modified to 13m clock, I can read and write the file correctly.

yacheng_zhang_1-1684218808334.png

yacheng_zhang_0-1684218557430.png

Here is my schematic diagram of the circuit,I tried to add resistance on the CLK line, but it didn't work.

 

Who can tell me where my problem is.

thank you

 

yacheng_zhang_2-1684218907839.png

 

 

 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,748件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

When you using the 52m, how about the log file of the board boot up?

0 件の賞賛
返信

1,719件の閲覧回数
yacheng_zhang
Contributor I

Maybe I found some reasons. I used emmc5.1. the official board was emmc4.44. Is there a difference between the voltage configuration of the imx6q? Do you have a reference circuit for the emmc5.1 chip with imx6q.

 

I tested the voltage of the emml clk only 2.0v.but the official board was 3.3v.what caused the difference.

0 件の賞賛
返信

1,695件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

The design is the same, here which version BSP are you using?

0 件の賞賛
返信