imx6q boot from emmc failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q boot from emmc failed

1,756 Views
yacheng_zhang
Contributor I

Hello, technical support:

      I made a imx6q board,When emmc works at 52m clock, it can't start properly. Manually modified to 13m clock, I can read and write the file correctly.

yacheng_zhang_1-1684218808334.png

yacheng_zhang_0-1684218557430.png

Here is my schematic diagram of the circuit,I tried to add resistance on the CLK line, but it didn't work.

 

Who can tell me where my problem is.

thank you

 

yacheng_zhang_2-1684218907839.png

 

 

 

Labels (1)
0 Kudos
Reply
3 Replies

1,745 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

When you using the 52m, how about the log file of the board boot up?

0 Kudos
Reply

1,716 Views
yacheng_zhang
Contributor I

Maybe I found some reasons. I used emmc5.1. the official board was emmc4.44. Is there a difference between the voltage configuration of the imx6q? Do you have a reference circuit for the emmc5.1 chip with imx6q.

 

I tested the voltage of the emml clk only 2.0v.but the official board was 3.3v.what caused the difference.

0 Kudos
Reply

1,692 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

The design is the same, here which version BSP are you using?

0 Kudos
Reply