imx6q android system reboot issue on Android 4.3 after several seconds

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q android system reboot issue on Android 4.3 after several seconds

2,446 次查看
pfsang
Contributor IV

hi,  ALL

      i encountered a problem about system reboot after about 20s.(i set android sleep time to 30min)

      my cpu (imx6q) works at 1Ghz.

      when i operate android (like play video, touch the panel), the system do not reboot automatically.

      but  when i do nothing , the system will reboot after about 20s . (i have tested several times).

      i also tried it on imx6DL, it has not the phenomenon .

      i have attached the log.

      by the way , i haven't ported pmic into the system. does it cause the reboot?

      do anyone give me suggest about how to debug it or what's the root cause?

 

 

Thanks

peter

Original Attachment has been moved to: after_20s_reboot.txt.zip

Original Attachment has been moved to: logcat_and_boot_log.txt.zip

标签 (5)
0 项奖励
回复
5 回复数

1,904 次查看
SergioSolis
NXP Employee
NXP Employee

Does it reboot even if you stop autoboot?, or is it only rebooting when you let android start?

0 项奖励
回复

1,904 次查看
pfsang
Contributor IV

hi, SerchMX

         >>  Does it reboot even if you stop autoboot?

             i don't stop autoboot and how to stop it?

         >>or is it only rebooting when you let android start?

             under linux , it do not reboot ,however under android , after the system start , if i do not any operation in about 20s , it will reboot .

0 项奖励
回复

1,904 次查看
SergioSolis
NXP Employee
NXP Employee

Is it a custom board you have? Have you ported the PMIC?, are you still having this issue?

0 项奖励
回复

1,904 次查看
saurabh206
Senior Contributor III

Hi,

Can you provide logcat detail?

And also check "developer options --> stay awake"  and "Display --> sleep time"

Saurabh

0 项奖励
回复

1,904 次查看
pfsang
Contributor IV

hi, Sauraph Patel

      Sorry to reply so late to you.

       i set "Display --> sleep time" to 30min and stay awake to disable

        and i added the logcat log

thanks

peter

0 项奖励
回复