imx6q SNVS 256-bit Master Key

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q SNVS 256-bit Master Key

1,587 Views
yilingxu
Contributor III

In Imx6q Security Reference Manual Chapter 6, see following:

If the SNVS determines the chip is in a trustworthy state, it allows CAAM to use a secret 256-bit value that CAAM uses to derive cryptographic keys during blob encapsulation and decapsulation.

We can know CAAM use 256-bit secret value to devrie cryptographic key blob encapsulation and decapsulation.

I want to confim if only CAAM can read this 256-bit secret value from SNVS? If not, except CAAM, who can read this 256-bit secret value from SNVS?

Labels (2)
0 Kudos
Reply
1 Reply

1,496 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent some comments directly.


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply