imx6q SNVS 256-bit Master Key

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q SNVS 256-bit Master Key

1,580 次查看
yilingxu
Contributor III

In Imx6q Security Reference Manual Chapter 6, see following:

If the SNVS determines the chip is in a trustworthy state, it allows CAAM to use a secret 256-bit value that CAAM uses to derive cryptographic keys during blob encapsulation and decapsulation.

We can know CAAM use 256-bit secret value to devrie cryptographic key blob encapsulation and decapsulation.

I want to confim if only CAAM can read this 256-bit secret value from SNVS? If not, except CAAM, who can read this 256-bit secret value from SNVS?

标签 (2)
0 项奖励
回复
1 回复

1,489 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent some comments directly.


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 项奖励
回复