imx6dl sending cmd1 to emmc not getting any response

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6dl sending cmd1 to emmc not getting any response

4,162 Views
swapniltiwari
Contributor II

in our custom based board we are using MT29PZZZ8D5BKFTF-18 W.95L(8gb emmc)4.51

when i am sending cmd0 then cmd1 to my emmc using jtag and i am not getting any response

for cmd1 i am probing cmd line which shows command trigger but no response after 56cycles also

i checked clock and power all seems good.what could be the reason of this kind of behaviour.

regards

swapnil

Labels (1)
7 Replies

3,006 Views
igorpadykov
NXP Employee
NXP Employee

Hi swapnil

usually such behaviour is caused by hardware: broken lines or missing

power, suggest to check emmc signals with oscilloscope.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,006 Views
swapniltiwari
Contributor II

Hi igor,

power lines,clocks and cmd line are all proper showing using osciiloscope

any other reason that i could look into?any basic steps specific to imx6dl

regards

swapnil

0 Kudos
Reply

3,006 Views
igorpadykov
NXP Employee
NXP Employee

Hi swapnil

one can try basic usdhc test in attached example from sdk.

Best regards

igor

3,006 Views
swapniltiwari
Contributor II

Hi igor,

i am using trace32 and cmm file in card identification mode but not getting

response from cmd1. Can you pls check my cmm file configuration

; --------------------------------------------------------------------------------

; @Title: i.MX6 eMMC FLASH Programming Script

; @Description:

;   FLASH Type: eMMC FLASH(Numonyx, NAND16GAH0P) connected SDHC3

;

;   S(D)RAM: 0x900000

;   SDHC CS3 base: 0x2198000

;

; @Author: jjeong

; @Chip: IMX6SOLO

; @Keywords: MACRONIX MX25L25635F

; @Copyright: (C) 1989-2014 Lauterbach GmbH, licensed for use with TRACE32(R) only

; --------------------------------------------------------------------------------

; $Id: imx6solo-emmc.cmm 2881 2014-07-07 10:35:48Z kjmal $

&MMC_BASE=0x2198000

  RESet

  SYStem.CPU iMX6Solo  ;SOLO

  ;CORE.ASSIGN 1        ;SOLO

  SYStem.Option ResBreak OFF

  SYStem.Option WaitReset 1.3s

  Trace.METHOD Onchip

  SYStem.Up

  Data.Set C15:0x1 %Long  (Data.Long(C15:0x1)&~(0x10005))  ; disable interrupt and mmu

  Data.Set ASD:0x020d8000 %Long 0x01C00521  ;SRC Control Register

; --------------------------------------------------------------------------------

; Disable WDOG

; --------------------------------------------------------------------------------

Data.Set 0x020bc000 %Word 0x30

; --------------------------------------------------------------------------------

; Enable all clocks (they are disabled by ROM code)

; --------------------------------------------------------------------------------

Data.Set 0x020c4068 %Long 0xffffffff

Data.Set 0x020c406c %Long 0xffffffff

Data.Set 0x020c4070 %Long 0xffffffff

Data.Set 0x020c4074 %Long 0xffffffff

Data.Set 0x020c4078 %Long 0xffffffff

Data.Set 0x020c407c %Long 0xffffffff

Data.Set 0x020c4080 %Long 0xffffffff

Data.Set 0x020c4084 %Long 0xffffffff

; --------------------------------------------------------------------------------

; IO Mux for SDHC3

; --------------------------------------------------------------------------------

Data.Set 0x020E030C %LE %Long 0x0  ;IOMUXC_SW_MUX_CTL_PAD_SD3_CLK

Data.Set 0x020E0310 %LE %Long 0x0  ;IOMUXC_SW_MUX_CTL_PAD_SD3_CMD

Data.Set 0x020E0314 %LE %Long 0x0  ;IOMUXC_SW_MUX_CTL_PAD_SD3_DAT0

Data.Set 0x020E06F4 %LE %Long 0x0001B0B0  ;IOMUXC_SW_PAD_CTL_PAD_SD3_CLK

Data.Set 0x020E06F8 %LE %Long 0x0001B0B0  ;IOMUXC_SW_PAD_CTL_PAD_SD3_CMD

Data.Set 0x020E06FC %LE %Long 0x0001B0B0  ;IOMUXC_SW_PAD_CTL_PAD_SD3_DAT0

; --------------------------------------------------------------------------------

; Config SDHC

; --------------------------------------------------------------------------------

Data.Set &MMC_BASE+0x04 %LE %Long 0x00010200  ; blk size,cnt

Data.Set &MMC_BASE+0x28 %LE %Long 0x08800020  ; bus width, endian

Data.Set &MMC_BASE+0x2C %LE %Long 0x008E1088  ; 400KHz clk

//FLASH READ ID TEST

AREA.CLEAR

AREA.view

GOSUB READ_ID_TEST

DIALOG.YESNO "the flash id is correct on AREA window?"

ENTRY &result

IF !&result

(

PRINT "pls, check your register configuration to enable your flash controller"

ENDDO

)

//S(D)RAM TEST for algorithm file

;GOSUB SDRAM_INIT

Data.Test 0x900000++0x3FFF  /Prime ;s(d)ram test

IF FOUND()

(

PRINT "s(d)ram is NOT initialized around 0x" ADDRESS.OFFSET(TRACK.ADDRESS())

ENDDO

)

programFlash:

FLASHFILE.RESet

;FLASHFILE.CONFIG  <eMMC controller> <#partition>  <0x0>

FLASHFILE.CONFIG  &MMC_BASE         0x0

;FLASHFILE.TARGET <<code range>> <<data range>> <<algorithm file>>

  FLASHFILE.TARGET  0x900000++0x1fff   0x904000++0x1fff   ~~/demo/arm/flash/byte/emmc_imx6.bin  /KEEP

  FLASHFILE.GETID

  Data.Set &MMC_BASE+0x2C %LE %Long 0x008E0188  ; 25Mhz clk, only allowed the data access commands on the higher clk

//Read FLASH Manufacture and Device ID

  FLASHFILE.DUMP 0x0               ; Read 

;FLASHFILE.ERASE 0x0--0xFFFFF     ; Erase

;FLASHFILE.LOAD * 0x0             ; Write

ENDDO

READ_ID_TEST:

//CMD0

RePeaT 2.

(

Data.Set &MMC_BASE+0x30 %Long 0xFFFFFFFF ;clear status

Data.Set &MMC_BASE+0x8 %Long 0x0  ;arg

Data.Set &MMC_BASE+0xc %Long 0x0  ;cmd

WAIT 10.ms

)

//CMD1

RePeaT 10.

(

Data.Set &MMC_BASE+0x30 %Long 0xFFFFFFFF ;clear status

Data.Set &MMC_BASE+0x8 %Long 0x40FF8000 ;arg

Data.Set &MMC_BASE+0xc %Long 0x01020000 ;cmd1

&resp=Data.Long(A:(&MMC_BASE+0x10))

//print "CMD1 resp: 0x" &resp

IF (&resp&0x80000000)==0x80000000

(

GOTO jump_cmd2

)

)

PRINT "CMD1 fail"

END

jump_cmd2:

//CMD2

Data.Set &MMC_BASE+0x30 %Long 0xFFFFFFFF ;clear status

Data.Set &MMC_BASE+0x8 %Long 0x0     ;arg

Data.Set &MMC_BASE+0xc %Long 0x02010000 ;cmd2

WAIT 10.ms

//CMD3

Data.Set &MMC_BASE+0x30 %Long 0xFFFFFFFF ;clear status

Data.Set &MMC_BASE+0x8 %Long 0x00010000  ; arg, MMC RCA is (0x0001<<16.)

Data.Set &MMC_BASE+0xc %Long 0x03020000  ;cmd3

WAIT 10.ms

//CMD10

Data.Set &MMC_BASE+0x30 %Long 0xFFFFFFFF ;clear status

Data.Set &MMC_BASE+0x8 %Long 0x00010000 ; arg, MMC RCA is (0x0001<<16.)

Data.Set &MMC_BASE+0xc %Long 0x0A010000  ;cmd10

WAIT 10.ms

//Response2

PRINT "CID register"

PRINT "[127:104] 0x" Data.Long(A:(&MMC_BASE+0x1c))

PRINT "[103:72]  0x" Data.Long(A:(&MMC_BASE+0x18))

PRINT "[71:40]   0x" Data.Long(A:(&MMC_BASE+0x14))

PRINT "[39:8]    0x" Data.Long(A:(&MMC_BASE+0x10))

RETURN

SDRAM_INIT:

RETURN

0 Kudos
Reply

3,006 Views
igorpadykov
NXP Employee
NXP Employee

Hi swapnil

you can look at attached cmm file and add there necessary codes.

Best regards

igor

0 Kudos
Reply

3,006 Views
swapniltiwari
Contributor II

Hi igor,

do you have any reference cmm file for emmc whatever you have attached is for ddr3

regards

swapnil

0 Kudos
Reply

3,006 Views
igorpadykov
NXP Employee
NXP Employee

Hi swapnil

no. Also suggest to check that SION bit was set in control pads, like

IOMUXC_SW_PAD_CTL_PAD_SD2_CLK, IOMUXC_SW_PAD_CTL_PAD_SD2_CMD

Best regards

igor

0 Kudos
Reply