Hello,
we have to support am 1280x800 display with single lvds channel. A display clock with 68 MHz is required. We're using the 3.10.17 kernel.
Everthing is ok when i set the pixel clock to 42.5 MHz and below. Higher clocks do not work but should since the imx6dl should deliver 85 MHz.
Thank you for helping.
Best regards,
Ludwig
已解决! 转到解答。
Hi Ludwig
LDB clock can provide up to 85 MHz.
Please check your clock tree. Set correct parent clock according to your requirement.