imx6d+ IPU virtual channels?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6d+ IPU virtual channels?

1,542 次查看
RandyKrakora
NXP Employee
NXP Employee

Customer is Aptiv.

They have a design with imx6d+, with connections as follows:

Parallel0 <- HDMI1

Parallel1 <- HDMI2

mipi-csi0 <- three inputs muxed through a lattice fpga - each using a different virtual channel.

Will the imx6d+ have the throughput to input and seperate all three inputs from the lattice at the same time? Assuming 720p resolution?

Regards,

Randy Krakora

0 项奖励
回复
1 回复

1,424 次查看
joanxie
NXP TechSupport
NXP TechSupport

do you need 2CSI+3MIPI? current bsp can support up to 4-CAMERA

The 4 cameras can be:

- 1xCSI, 3xMIPI

- 2xCSI, 2xMIPI

- 4xMIPI

more detailed settings, pls refer to the document as below:

https://community.nxp.com/docs/DOC-328548?commentID=55362#comment-55362 

0 项奖励
回复