imx6Ul RTC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6Ul RTC

1,564件の閲覧回数
小辉哥
Contributor III

你好,imx6ul rtc 电池供电的时候那个R1 ,1k电阻是做什么用的,为什么要加一个电阻,可以去掉吗?

pastedImage_1.png

ラベル(3)
0 件の賞賛
返信
1 返信

1,364件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

 The resistor is intended to restrict charge current, if chargeable battery is applied:

“Appropriate series resistor (Rs) must be used when connecting the coin cell. Rs depends

on the charge current limit that depends on the chosen coin cell.”

   Refer to section, named OSC32K in i.MX 6UL Datasheet(s), for more details.

https://www.nxp.com/docs/en/data-sheet/IMX6ULCEC.pdf 

 

  So, the Rs resistor may be removed if non- chargeable battery is used in Your design.

Note, if diode D2 is used, R1 resistor is not required and vice versa. 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 件の賞賛
返信