imx6ULL HAB keys

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ULL HAB keys

1,983 Views
parthitce
Contributor III

Hello Yuri,

Thanks for sharing that ERRATA details. I will check it. Unfortunately I am already using Engine = SW, this ERRATA should not affect my case.

I have another question here,
- Will it be possible to change the HAB keys? For example, I have fused a keys in bank 3 words 0 - 7 and found it isn't working and I want to change to new keys.

Or the fuses always one time programmable for bank 3 words 0 - 7?

In my case, I tried changing it couple of times with different keys and now I am not able to read the keys which I write into it at all using "fuse read". I also noticed that "fuse override" just overrides the shadow registers for testing purpose, but not change the real fuse.

Thanks in advance,

Parthiban N

1 Reply

1,914 Views
Yuri
NXP Employee
NXP Employee

 

Hello,

 

  The i.MX fuses can be burned once.

    But customers can use the revoke feature, described in Appendix B

(SRK revocation on i.MX 6 & 7 series) of "Secure Boot on i.MX 50, i.MX 53,

i.MX 6 and i.MX 7 Series using HABv4" Application Note, Rev. 2, 05/2018

 

https://www.nxp.com/docs/en/application-note/AN4581.pdf 

Have a great day,

Yuri

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.