imx6DL AndroidN mfgtool image build

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6DL AndroidN mfgtool image build

1,811 Views
jiujinhong
Contributor IV

Hi,

We want to build androidN mfgtool image in AndroidN BSP(Kernel 4.1.15, Uboot 2015.4),  How to build? 

Currently the mfgtool image we use is from others.  Because of  hardware change(Memory capacitiy),  means we need to build new mfgtool image.  Look through all documents from fsl,  there are no any chapter about how to build mfgtool image in Android N BSP and there are no *mfgconfig in code level, Please tell us how to fix this issue.  Yocto image and development env are very large and we don't want to setup it and build  image, duplicate work.

0 Kudos
Reply
2 Replies

1,702 Views
igorpadykov
NXP Employee
NXP Employee

Hi jiu

steps for rebuilding mfg tool are given in sect.6.2 Manufacturing Tool, MFGTool

attached Yocto Guide, steps are the same for android. Sources should be modified

for custom board: change drivers, change ddr calibration coefficents after running ddr test

i.MX6/7 DDR Stress Test Tool V2.90 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,702 Views
jiujinhong
Contributor IV

That means we need to maintain stupid duplicate development work to support mfgtool image.

0 Kudos
Reply