Hi all,
on our project, we have a 4.19.35 kernel, based on meta-fsl-bsp-release.
we have an video decoder isl79987 with 4 analogic camera.
We have applied the patch from this url:
iMX6DQ ISL79985/79987 MIPI CSI2 CVBS camera surround view solution for Linux BSP
and we use mxc_v4l_tvin.out test application.
Everything works well, we are able to display 4 camera stream on a hdmi screen.
Our question is related to the test application.
Indeed, we see that in this application, direct access is done to the ipu driver, but when we look at the imx-test mxc_v4l2_capture.c (here: mxc_ipudev_test.c\mxc_ipudev_test\test - imx-test - i.MX Driver Test Application Software )
we see that everything use the v4l2 framework.
So i would like to know if it is better using v4l2, or direct using ipu driver (is there better performance using ipu directly, or through v4l2)?
Is the mxc_v4l_tvin application test stored on a git repo somewhere?
Thanks in advance for your answer
Regards
Laurent