imx6 ubifs sqnum error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 ubifs sqnum error

ソリューションへジャンプ
4,789件の閲覧回数
XiaofengZang
Contributor III

Hello

imx6 linux ubifs system found sqnum error after using 3 months, the rootfs is read only.

log is in attachment,why bad replay sqnum is smaller than commit sqnum?

it should be bigger than commit forever 

[ 2.994248] UBIFS error (ubi0:0 pid 1): replay_log_leb: bad sqnum 1050630, commit sqnum 1068183
[ 3.002967] UBIFS error (ubi0:0 pid 1): replay_log_leb: log error detected while replaying the log at LEB 6:2048

ラベル(2)
0 件の賞賛
返信
1 解決策
4,600件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Xiaofeng

one can try with latest nxp linux releases from Code Aurora git repositories  repository

linux-imx - i.MX Linux kernel 

Documentation i.MX Software | NXP 

also (to exclude quality issue) one can try with other nand part form another vendor.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,601件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Xiaofeng

one can try with latest nxp linux releases from Code Aurora git repositories  repository

linux-imx - i.MX Linux kernel 

Documentation i.MX Software | NXP 

also (to exclude quality issue) one can try with other nand part form another vendor.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,600件の閲覧回数
XiaofengZang
Contributor III

Hi

this reason is nand driver update, our version is 4.1.15, it's too old.

0 件の賞賛
返信
4,297件の閲覧回数
zhangzhencai
Contributor II

你好,我们这边也遇到相同的问题,请教一下你那边驱动升级了哪些文件。能打个压缩包,我们这边参考一下吗?

UBIFS (ubi0:0): background thread "ubifs_bgt0_0" stops
UBIFS (ubi0:0): recovery needed
UBIFS error (ubi0:0 pid 1): replay_log_leb: bad sqnum 72163, commit sqnum 72714
UBIFS error (ubi0:0 pid 1): replay_log_leb: log error detected while replaying the log at LEB 5:2048

0 件の賞賛
返信