imx6 quad thermal analysis

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 quad thermal analysis

1,298 Views
abhaykumar_sing
Contributor I

Hi,

I need to perform thermal analysis for IMX6 Quad core.

How can i enable and stress all applicable peripherals and also Is there some Stress Tool available to Stress the Cores of the IMX6 processor?

0 Kudos
Reply
1 Reply

1,243 Views
igorpadykov
NXP Employee
NXP Employee

Hi abhay

unfortunately such special tools or images are not available.

In general one can try Demo image with a gui from below link

and run some high resolution video or graphics, this will stress

most of processor peripherals

i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply