imx6 mfg image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 mfg image

6,060 Views
玉栋郭
Contributor III

hi ~

 各位,我正在使用MFG tool ,使用说明里(Manufacturing Tool V2 Quick Start Guide.docx)

How to Burn Your Own Image with Manufacturing Tool

The processes above are limited to the reference design boards provided by Freescale. All the U-Boot images and kernel images are used to support Freescale reference design boards. If you want to utilize the tool to burn your own image on your own board, all you need to do is the following:

  • Generate a special U-Boot image and kernel image for MFG tool
  • Generate a normal U-Boot image and kernel image, maybe customizing rootfs which can be used by the end user.
  • Refer to the ucl2.xml to create your own operation list. Usually, only changing the original image (U-Boot and kernel) is enough.

The detailed information about how to generate Manufacturing firmware, refer to the Document “Manufacturing Tool v2 Linux or Android Firmware Development Guide.”

其中

  • Generate a special U-Boot image and kernel image for MFG tool

请问一下,special U-Boot image and kernel image  for MFG tool  和  normal U-Boot image and kernel image  有什么区别? 我能直接使用normal image 代替 special image吗?

Labels (2)
Tags (1)
0 Kudos
Reply
7 Replies

5,428 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

About the mfgtool describe you can read the document in mfgtool.

0 Kudos
Reply

5,428 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You can use target board uboot on MFG tool. There is not difference on uboot. Kernel only have difference for MFGTool

0 Kudos
Reply

5,428 Views
玉栋郭
Contributor III

hi  Rita Wang

因为我用的并不是yocto,我单独编译的kernel,我想知道mfg kernel 和 normal kernel  哪个地方不一样?然后我有针对性的修改。

0 Kudos
Reply

5,428 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

OK, I know what do you want, here could you please tell me which version BSP are you using first?
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,428 Views
玉栋郭
Contributor III

hi  Rita Wang

 我用的是fsl_yocto-L4.1.15_2.0.0-ga 这个。

0 Kudos
Reply

5,428 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You can refer to the follwing document,

6.2 Manufacturing Tool, MFGTool
One way to place an image on a device is to use the MFGTool. The recipes used to build a manufacturing tool image are
linux-imx-mfgtool and u-boot-mfgtool.
To build a manufacturing image do the following -
$ bitbake fsl-image-mfgtool-initramfs


Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,428 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Which BSP are you using? If you design the board yourself, you need to build the images for mfgtool. The default mfgtool is working for our reference board. Here you can use the same images. They will work fine.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply