imx6+isl79987

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6+isl79987

2,218 Views
xiaojunye
Contributor I

Hi,

      有个问题想请教一下,主板mx6q,内核30.035,isl79987与mx6q通过2 lanes mipi连接。

现在isl79987 与mx6q i2c通信正常,但是示波器测量不到mipi 时钟信号,打印“mipi csi2 can not receive sensor clk! MIPI_CSI_PHY_STATE = 0x200”,请问有遇到过吗?怎么解决的

0 Kudos
Reply
1 Reply

1,931 Views
igorpadykov
NXP Employee
NXP Employee

Hi xiaojun

please try to adjust clock following steps described on

Debug steps for customer MIPI sensor.docx 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply