imx6 increase sched_clock resolution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 increase sched_clock resolution

2,659件の閲覧回数
arashjavanmard
Contributor I

Hi,

My Env.:

Board: Boundary Device Nitrogen Max

Kernel: 3.14.28

OS:  Debian 8

right now my Sched_clock read from dmesg is:

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns

how/where in kernel source can i increase the timer resolution?

thanks

タグ(3)
0 件の賞賛
返信
1 返信

2,496件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi arash

please refer to attached Linux Manual

sect.3.3.3 Timer Source Code Structure

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信