imx6 increase sched_clock resolution

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6 increase sched_clock resolution

2,625 次查看
arashjavanmard
Contributor I

Hi,

My Env.:

Board: Boundary Device Nitrogen Max

Kernel: 3.14.28

OS:  Debian 8

right now my Sched_clock read from dmesg is:

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns

how/where in kernel source can i increase the timer resolution?

thanks

标记 (3)
0 项奖励
回复
1 回复

2,462 次查看
igorpadykov
NXP Employee
NXP Employee

Hi arash

please refer to attached Linux Manual

sect.3.3.3 Timer Source Code Structure

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复