imx6 encoder decoder test binaries generated in buildroot not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 encoder decoder test binaries generated in buildroot not working

1,686件の閲覧回数
adityanagal
Contributor III

Hi ,

I am using buildroot and cross-compiling the imx-mm library using linaro toolchain. The encoder and decoder not working on the imx6 target board . Binaries name is example test_mp3_dev_arm9_elinux_fhw .

Doen anybody have the clue , why these binaires are not working ?

Thanks

Aditya Nagal

0 件の賞賛
返信
2 返答(返信)

1,631件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Please use the tests package, say mxc_vpu_test. 

http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 件の賞賛
返信

1,631件の閲覧回数
adityanagal
Contributor III

Thanks for your reply but this link does not have the audio encoders and decoder. Could you please provide me the source using which I can test the Audio encoders and decoders possibly using IMX-mm or gst-fsl-plugin library,

Regards,

Aditya Nagal

0 件の賞賛
返信