imx6 encoder decoder test binaries generated in buildroot not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6 encoder decoder test binaries generated in buildroot not working

1,671 次查看
adityanagal
Contributor III

Hi ,

I am using buildroot and cross-compiling the imx-mm library using linaro toolchain. The encoder and decoder not working on the imx6 target board . Binaries name is example test_mp3_dev_arm9_elinux_fhw .

Doen anybody have the clue , why these binaires are not working ?

Thanks

Aditya Nagal

0 项奖励
回复
2 回复数

1,616 次查看
Yuri
NXP Employee
NXP Employee

Hello,

Please use the tests package, say mxc_vpu_test. 

http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 项奖励
回复

1,616 次查看
adityanagal
Contributor III

Thanks for your reply but this link does not have the audio encoders and decoder. Could you please provide me the source using which I can test the Audio encoders and decoders possibly using IMX-mm or gst-fsl-plugin library,

Regards,

Aditya Nagal

0 项奖励
回复