imx6 camera interface I/O voltage levels

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6 camera interface I/O voltage levels

1,330 次查看
erdempamuk
Contributor I

hi guys

does imx6 camera interface I/O  s are  2.8V ? or 1.8V ?

0 项奖励
回复
1 回复

1,114 次查看
igorpadykov
NXP Employee
NXP Employee

Hi erdem

NVCC_CSI can be from 1.65 to 3.6V

please check Table 6 "Operating Ranges'

IMX6DQCEC i.MX 6Dual/6Quad Applications Processors for Consumer Products - Data Sheet

One can also check sect.4.6.2 "General Purpose I/O (GPIO) DC Parameters",

Table 100 "21 x 21 mm Functional Contact Assignments".

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复