imx6-SDP onBoard eMMC Detection on WEC7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6-SDP onBoard eMMC Detection on WEC7

ソリューションへジャンプ
2,045件の閲覧回数
TugrulGuclu
Fresh Out Contributor

    Hi

I have imx6-QuadCore SDP and runnig WEC7 on it.

I'm trying to run CTK file system performance test on on board eMMC (index=4) but no matter how SDHC driver can not detect the card.

I can not see it as a storage medium on explorer.exe

Any ideas about the problem ?

Thanks

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,774件の閲覧回数
dmitriyaleksand
Contributor II

Hi,

eMMC does not have Card Detect pin, so you need to patch SD Card driver to inform it that SD Card is always present in this slot.

Regards,

Dmitriy

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,775件の閲覧回数
dmitriyaleksand
Contributor II

Hi,

eMMC does not have Card Detect pin, so you need to patch SD Card driver to inform it that SD Card is always present in this slot.

Regards,

Dmitriy

0 件の賞賛
返信