imx6: BSP yocto with old uboot from BSP 4.0.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6: BSP yocto with old uboot from BSP 4.0.0

720件の閲覧回数
mralmond
Contributor II

Is it possible to boot the new BSP yocto (kernel 3.10.17 and new rootfs) using the old uboot from the old BSP version 4.0.0 (the one with kernel 3.0.35)?

I'm asking this because I need to perform an update from user interface of a board running the old BSP and I'd like to avoid updating also the bootloader (for security/stability reasons).

Thank you.

ラベル(3)
1 返信

565件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Gianluca,

     According to the function of bootloader, it is possible to use old u-boot to load new linux kernel, but I don't recommend you do like this. You konw, since linux 3.10.x, the architecture of linux driver has been changed completely, correspondingly, bootloader was also updated, as for security & stability , new bootloader should be better than old one, so I suggest you'd better port new BSP including u-boot to your board completely !

Hope above suggestions can help you !

If these suggestions are helpful for you, click "correct" botton or "helpful" button to close the ticket!

Regards,

Weidong