imx6 Android IPU VDI mode motion 0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6 Android IPU VDI mode motion 0

1,450 次查看
notyet
Contributor I

Hi.

I'd like to set VDI mode motion 0 on the Android BSP with below source.

How could I do it???

 

According to Doc :
i.MX6 IPU TVIN Application Note

 

4.3 On The Fly De-interlace
Except for the memory to memory de-interlace, the IPU can also support on the fly de-interlace
with CSI->VDI->MEM (g_input = 3 with VIDIOC_S_INPUT) and CSI->VDI->IC->MEM (g_input = 2
with VIDIOC_S_INPUT) capture path: https://community.nxp.com/docs/DOC-330441

Limitations:
1. Since the IC can only output resolution up to 1024*1024, so this is the limitation on output for
CSI->VDI->IC->MEM path.
2. Since the VDI can only output resolution up to 968*1024, so CSI->VDI->MEM can’t work for
1080i capture.
3. Only VDI motion mode 2 was supported. To avoid dithering, the driver should set one field
data for CSI->VDI->xxx path, set VDI_SKIP and VDI_MAX_RATIO_SKIP to 1 in register
IPU_SKIP.

Note: The reason to set VDI_SKIP to skip one field data, ODD field starts from line 1 and EVEN
field starts from line2, so they are one line shift, if the VDI using both field data, the output video will
dithering between switching ODD and EVEN field.

0 项奖励
回复
1 回复

1,432 次查看
igorpadykov
NXP Employee
NXP Employee

Hi notyet

 

for "VDI mode motion 0" one can refer to liniux vdi driver, in particular function void _ipu_vdi_set_motion():

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/mxc/ipu3/ipu_ic.c?h=imx_5.4.47_2.2...
https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/gpu/imx/ipu-v3/ipu-vdi.c?h=imx_5.4...

 

Best regards
igor

0 项奖励
回复