imx6 3.10.17fsl: Patch to support uboot logo keep from uboot to kernel (LCD and LVDS)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 3.10.17fsl: Patch to support uboot logo keep from uboot to kernel (LCD and LVDS)

1,363 Views
cniedermaier
Contributor III

Hello,

is there a patch for the freescale Kernel 3.10.17 to made the display no interrupt from uboot to kernel (LCD and LVDS)?

A similar patch is available for Android (JB4.2.2_1.1.0-GA and L3.0.35_4.1.0-GA BSP):

https://community.freescale.com/docs/DOC-98109

Thanks in advance!

Best Regards,

Christoph

Labels (2)
0 Kudos
Reply
2 Replies

837 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Christoph,

     You can port boot LOGO from patch for L3.0.35_4.1.0-GA BSP to 3.10.17, the procedure is not difficult , because it is from one u-boot to another u-boot.

Regards,

Weidong

0 Kudos
Reply

837 Views
cniedermaier
Contributor III

Hi Weidong,

unless I'm wrong you have to patch both u-boot and the kernel.

I think the patches for the kernel are for version 3.0.35 and not for 3.10.17.

The patches won't apply, because the structure of the kernel changed a lot (e.g. board file --> device tree)

Best Regards,

Christoph

0 Kudos
Reply