hi,
I was tested usb device in mx53 board and not working device mode.
My Menuconfig settings are here below.
First one i was set for following menuconfig settings:
"CONFIG_MXC_OTG, CONFIG_USB_OTG\n
"CONFIG_USB_EHCI_ARC_OTG\n"
"OTG device config\n"
"CONFIG_USB_GADGET\n"
I got in serial port/console message while i was insert and remove in USB device cable(J3).
usb wakeup is here
otg host ID wakeup
hub 1-0:1.0: activate --> -22
usb wakeup is here
otg host ID wakeup
also usb driver not installed in this settings
second one i was set USB device mode settings and udb driver not installed .
"CONFIG_USB_GADGET\n"
in device mode was not working and if any settings are missing compare to above device mode configuration please tell me the correct procedure to enable imx53qsb device mode .
已解决! 转到解答。
Hello,Venkatesh,
On i.mx53QSB board, USB OTG is designed as Dual Role ( device or Host), Device function is at MicroUSB Connector, Host function is at the bottom one on USB host connector.
Two functions can't be used simutinously !
In addition, when connecting USB OTG to USB HOST on PC, driver should be installed. this driver is released with MFG Tools by Freescale. So please download MFG Tools From Freescale formal website.
Only After you install this driver, i.MX53QSB can be used as a USB OTG device.
Regards,
Weidong
hi Krakora,
The above link method not detecting USB Device Mode.......let me know any other settings means please tell me.
Any Menuconfig settings for to enable device mode.
Thanks by,
Venkatesh.P
Hello,Venkatesh,
On i.mx53QSB board, USB OTG is designed as Dual Role ( device or Host), Device function is at MicroUSB Connector, Host function is at the bottom one on USB host connector.
Two functions can't be used simutinously !
In addition, when connecting USB OTG to USB HOST on PC, driver should be installed. this driver is released with MFG Tools by Freescale. So please download MFG Tools From Freescale formal website.
Only After you install this driver, i.MX53QSB can be used as a USB OTG device.
Regards,
Weidong