imx53qsb usb device not working and how to enable the device mode in mx535qsb board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx53qsb usb device not working and how to enable the device mode in mx535qsb board.

Jump to solution
1,480 Views
venkatesh_pvsm
Contributor II

hi,

   I was tested usb device in mx53 board and not working device mode.

My Menuconfig settings are here below.

First one i was set for following   menuconfig settings:

        "CONFIG_MXC_OTG, CONFIG_USB_OTG\n

        "CONFIG_USB_EHCI_ARC_OTG\n"

        "OTG device config\n"

        "CONFIG_USB_GADGET\n"

  I got in serial port/console message while i was insert and remove in USB device cable(J3).

usb wakeup is here

otg host ID wakeup

hub 1-0:1.0: activate --> -22

usb wakeup is here

otg host ID wakeup

also usb driver not installed in this settings

second  one i was set USB device mode  settings and udb driver not installed .

        "CONFIG_USB_GADGET\n"


in device mode was not working and if any settings are missing compare to above device mode configuration please  tell me the correct procedure to enable imx53qsb device mode .





Labels (1)
0 Kudos
Reply
1 Solution
1,039 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Venkatesh,

     On i.mx53QSB board, USB OTG is designed as Dual Role ( device or Host), Device function is at MicroUSB Connector, Host function is at the bottom one on USB host connector.

      Two functions can't be used simutinously !

      In addition, when connecting USB OTG to USB HOST on PC, driver should be installed. this driver is released with MFG Tools by Freescale. So please download MFG Tools From Freescale formal website.

      Only After you install this driver, i.MX53QSB can be used as a USB OTG device.

Regards,

Weidong

View solution in original post

0 Kudos
Reply
4 Replies
1,039 Views
venkatesh_pvsm
Contributor II

hi Krakora,

     The above link method not detecting USB Device Mode.......let me know any other settings means please tell me.

Any Menuconfig settings for to enable device mode.

Thanks by,

Venkatesh.P

0 Kudos
Reply
1,040 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Venkatesh,

     On i.mx53QSB board, USB OTG is designed as Dual Role ( device or Host), Device function is at MicroUSB Connector, Host function is at the bottom one on USB host connector.

      Two functions can't be used simutinously !

      In addition, when connecting USB OTG to USB HOST on PC, driver should be installed. this driver is released with MFG Tools by Freescale. So please download MFG Tools From Freescale formal website.

      Only After you install this driver, i.MX53QSB can be used as a USB OTG device.

Regards,

Weidong

0 Kudos
Reply
1,039 Views
venkatesh_pvsm
Contributor II

hi Weidon,

thanks for your reply.

0 Kudos
Reply
1,039 Views
RandyKrakora
NXP Employee
NXP Employee
0 Kudos
Reply